Hello every body,
I'm working on a board with a Kinetis K70, MQX4.2.
I would know if is exist a configurable library to implement the CanOpen Standard (DS301 and then DS401 because i'm working on a IO module)?
I need to work in master and in slave.
Is every body know an already done stack available?
Thank
Solved! Go to Solution.
Hello Arnaud,
CANopen is supported by a third party and have an extra cost.
Please check the following link:
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok
So no Free solution existing.
Thank you:smileywink: