AnsweredAssumed Answered

Bring up the custom imx6 dual board

Question asked by Le Tan on Nov 30, 2015
Latest reply on Dec 3, 2015 by Yuri Muhin

Hello together,

 

This is the first time I bring up so may imx6 hardwares for my customer . My hardware has:

  • MCIMX6D5EYM10AD imx6 dual; MT41K512M16HA-125 RAM; MTFC8GLCDM eMMC
  • jtag connector
  • uart 1

 

Below is my plan for bringing up:

  1. Flash DDR3 calibrate binary through JTAG (don't have u-boot this time)
  2. Run DDR3 binary and get the configs when calibrating DDR3
  3. Fill DDR3 configs to u-boot source code
  4. Porting u-boot to boot from eMMC

 

This is my questions related to the steps to bring up hardware:

  1. Which UART do I need to get the configuration when calibrating DDR3 stress test (UART1? or UART0?)
  2. Any driver for RAM MT41K512M16HA-125?
  3. Do I need driver for MTFC8GLCDM eMMC when bringing up?

 

Thanks,

Tan

Outcomes