Hello all,
I am having an issue writing and booting Ubuntu 10.04 to the iMX50. The issue is that the iMX50 will not boot from an SD card. The process I am following is:
RD3 U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 0 ${loadaddr} 0x800 0x1800;bootm'
RD3 U-Boot > setenv bootcmd 'run bootcmd_mmc'
7. Running bootm after this then returns
ERROR: can't get kernel image!
Any suggestions on how to fix this problem would be much appreciated
Thanks in advance,
Andrew
Hi Andrew
one can follow guidelines in sect.7.2 Run the image from MMC/SD flash
attached User Guide from BSP package:
Board Support Packages (4)
Linux 2.6.35 Source Code Files and documentation 2011.04 (REV 2011.04)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------