Loris Caren

M5235EVB dbug Set hangs

Discussion created by Loris Caren on Feb 6, 2008
Latest reply on Feb 8, 2008 by Tom Thompson
I've just started to use a new M5235EVB. When I try to use the set command, for example
set client 192.168.1.10, or set baud 19200 (the current baud), the dbug hangs and I only get a prompt back
if I reset. This surely isn't right? I haven't altered any of the DIP switches.
The firmware is v3b.1a.1a (Built on Aug 27 2004 16:16:25)
The boot prompt doesn't mention a DRAM size as the UM examples do.
Brief trial of other commands seem OK.

Outcomes