Hi Tech support,
I previously purchased CW USB TAP.
Probe Tip: Power Architecture JTAG/COP
PC window 7 64 bit.
PC installed Power Architecture 8.8
Target PCB with the processor: MPC8358ECVRAGDGA
It worked. Typed "findcc utaps" @ CCS, it shows my CW USB TAP serial number.
I am able to "erase" in flash programmer.
Problem:
I purchased CW TAP (Supports USB and Ethernet) for mass production.
PC window 7 64 bit. (Same)
PC installed Power Architecture 8.8 (Same)
Target PCB with the processor: MPC8358ECVRAGDGA (Same)
It failed. Typed "findcc utaps" or "findcc ethaps", etc @ CCS. It does not show anything.
I am NOT able to "erase" in flash programmer, it shows check JTAG clock speed.
i have set netparam as following:
core> netparam
ethernet_address = 00:04:9F:03:9B:ED
bootconfig = static:FSL039BED
static_ip_address = 169.254.3.4
static_dns_server = <none>
static_hosts = <none>
static_routes = <none>
PC directly connects to CW TAP.
PC's ip= 169.254.3.2
PC's subnet mask= 255.255.0.0
Please advise.
The correct command for finding cwtap in ccs is: findcc cwtaps. Because you are using an old version of CW, it is possible that your ccs version to not support cwtap. Here is a document showing how to update ccs for cwtap usage (it is not for your version of CW, but is applicable).
Adrian
Hi Adrian,
Which version should i use for supporting cwtap?
Current version is Power Architecture 8.8.
My company also has version Power Architecture 10.0.2. Does it support cwtap?
If not, which version should i get?
Thanks for the support.
Mario
Hi Mario,
The latest version of CodeWarrior is 10.5, and this is the version recommended. But, you can follow the steps from the doc, and use a version of ccs that supports cwtap in your CW 8.8 version.
Also, you can check if your PA 10.0.2 supports cwtap, by opening ccs and probe the command: findcc cwtaps.
Adrian