AnsweredAssumed Answered

Booting T4240RDB from SD card or SPI

Question asked by Michael Borgelt on Nov 27, 2015
Latest reply on Feb 5, 2016 by nick caruso

Hello all,

 

I am having quite a bit of trouble building a U-Boot, in Yocto (SDK 1.8) and then

deploying it onto an SD card and booting it on the T4240RDB eval board.

Since T4240RDB U-Boot does not support SDCARD I build T4240QDS_SDCARD.

I copied the generated file: u-boot-sd-T4240QDS_SDCARD-2014.07+fslgit-r0.bin
to block 8 of the SD-card and set T4240RDB SW2-1 to OFF (RCW in SD/EEPROM) and SW3-4
to ON (RCW source located in SD).
But this does not work. I also tried to
create the bin file using the QorIQ Configuration Suite but also without success.

Is there anyone who hast booted T4240RDB from SD-card or SPI?

 

Outcomes