What is the specifications to power up hdmi to vga signals with imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the specifications to power up hdmi to vga signals with imx6

432 Views
narasimhuluorug
Contributor III

Hello,

Is there any power limitations which is to power up the display monitor with hdmi to vga conversions ?

Thanks & Regards

narasimha

0 Kudos
1 Reply

361 Views
igorpadykov
NXP Employee
NXP Employee

Hi narasimha

there are no special limitations, in general first should be powered

processor, then external devices.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos