HI!
I`m using buildroot to produce runnable linux image for my imx23-based board. Now i need to set cpu freq at startup of the system to 392.73MHz.
I thought that it possible to do it with "cpufreq" utility but buildroot fails to compile it for imx23. Also i need to set ddr freq to 96MHz.
So can anybody show me way how to set cpu and ddr freqs of the system or advice something else?
HI Anatol
some such examples can be found in imx-bootlets_xx/boot_prep/init-mx23.c :
or i.MX23 ltib Linux 2.6.31 :
Recommended Software & Tools (5)
Linux 2.6.31 Source Code Files 2010.05 Release (REV 2010.05)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------