Can we use i.MX6 CLKx_P/CLKx_N for PLL clock source?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use i.MX6 CLKx_P/CLKx_N for PLL clock source?

Jump to solution
772 Views
satoshishimoda
Senior Contributor I

Hi community,

I havea a question about i.MX6 PLL.

Please see chapter 18.7.1 in IMX6DQRM Rev.3, we can select REF_CLK_24M, CLK1, CLK2, and XOR for bypass source.

Then, is this setting enabled when PLL is not bypass mode?

In other words, can we use CLKx_P/CLKx_N for PLL clock source not only in bypass mode but also normal mode?

Best Regards,

Satoshi Shimoda

Tags (2)
0 Kudos
1 Solution
661 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

CLKx_P/CLKx_N can not be used for PLL clock source.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
662 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

CLKx_P/CLKx_N can not be used for PLL clock source.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
661 Views
satoshishimoda
Senior Contributor I

Dear Igor,

Thank you for your prompt reply.

Ok, I understood CLKx_P/CLKx_N can be used for "bypass source" only.

Best Regards,

Satoshi Shimoda

0 Kudos