I just purchased a TWR-K60F120M kit. The Kinetis SDK does not have examples for this particular micro. I tried using the hello world example for twrk60d100m. The program hangs in fsl_msg_hal_modes.c executing the line while (!CLOCK_HAL_IsPll0Locked(base)) {}. I also tried using the example for the TWRK64f120m. This seemed to continuously reset the processor.
Is there an example for the processor I have, or is there a way to fix the problem with the example I am using?
Thanks.
Hello Ken,
Yes, the KSDK1.3 is the latest version now , and it have not support the board of TWR-K60120M.
I think you can also use the Processor Expert driver to development your project , and there are the component of
peripherals , it only need add them you need .
If you want use , when you create project , please select it :
For example , if you want use the print words through UART , you only need add the component of "ConsoleIO":
Hope it helps
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have a great day,
Alice
Hi Ken,
unfortunately there is no support in KSDK 1.3. for TWR-K60F120M.
But you can take a look at examples under MQX 4.2,
located here C:\Freescale\Freescale_MQX_4_2\mqx\examples
or you can try migrate your MCU for KSDK. I include you guide.
You find closest device, i.g. K64F120M and create device specific files, set compiler, create configuration files for the board and modify projects.
Hope this helps.
Iva
Hello Ken,
Please tell me which IDE do you use ? And what about the version of SDK ? And what hello world demo do you want , with SDK ? with PE ? with MQX ?
or others ?
BR
Alice
Hi Alice,
Thanks for your quick response. I am using version 3.0.0 of the Kinetis Design Studio IDE. I am using version 1.3.0 of the KSDK. I downloaded both of these this week, so I assume they are the latest. I would like the demo for both the SDK and MQX, though the SDK is the most important.
Thank you,
Ken