AnsweredAssumed Answered

Include paths not updating

Question asked by Michael Thomas on Nov 23, 2015
Latest reply on Dec 4, 2015 by Michael Thomas

I'm using KDS 3.0 and having a problem building my project due to paths not being updated.

IncludePath.png

Notice the "D4D" directory is in my include path.  However, when I compile the project, this path is not included in the search:

 

15:36:42 **** Build of configuration Debug for project NextGenUIM ****

make all

'Building file: ../Supervisory_Code_Level/MyMain.c'

'Invoking: Cross ARM C Compiler'

arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3

-I"C:/AOSGit/NextGenUIM/Static_Code/System"

-I"C:/AOSGit/NextGenUIM/Static_Code/PDD"

-I"C:/AOSGit/NextGenUIM/Static_Code/IO_Map"

-I"C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert/lib/Kinetis/pdd/inc"

-I"C:/AOSGit/NextGenUIM/Sources"

-I"C:/AOSGit/NextGenUIM/Generated_Code"

-I"C:/AOSGit/NextGenUIM/Static_Code/Peripherals"

-I"C:/AOSGit/NextGenUIM/Class_Code_Level"

-I"C:/AOSGit/NextGenUIM/Common_Headers"

-I"C:/AOSGit/NextGenUIM/Superclass_Code_Level"

-I"C:/AOSGit/NextGenUIM/Supervisory_Code_Level"

-std=c99 -MMD -MP -MF"Supervisory_Code_Level/MyMain.d" -MT"Supervisory_Code_Level/MyMain.o" -c -o "Supervisory_Code_Level/MyMain.o" "../Supervisory_Code_Level/MyMain.c"

../Supervisory_Code_Level/MyMain.c:20:17: fatal error: d4d.h: No such file or directory

#include "d4d.h"

                 ^

compilation terminated.

make: *** [Supervisory_Code_Level/MyMain.o] Error 1

 

How do I get KDS to recognize the new include path?

Outcomes