Question, i.MX28 clock input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX28 clock input

467 Views
Aemj
Contributor IV

Hi team,

I would like to ask about i.MX28 clock input.

My customer has started the HW design for their own i.MX28 board and they will use crystal for i.MX28 clock input.

Do you have any specification for clock input?

Duty cycles, deflection voltage range, etc.

The customer is trying to use a crystal which has about 560mV of deflection range.

Is it OK for i.MX28?

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Reply

385 Views
art
NXP Employee
NXP Employee

The i.MX28 processor has the internal oscillation circuits for both 32kHz and 24MHz clock sources. Both oscillation circuits are supplied from the internal linear voltage regulator that produces the VDDXTAL voltage whose typical value is 1.1V. The typical external crystal parameters are as per the specifications attached. The typical duty cycle is 50%.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos