I develop one application using code worrior 10.2 and mqx rtos.one part of this application dose following things
-erase one part of flash
-programme it
i am using standard c90fl flash driver .
on many board this application work fine but on some bord its stuck when erase command used.all voltages on such board is ok and even i can programme it using debugger.what should be the problem????
i am using mpc5668g controller and same driver i am using in one previous application which is not based on mqx rtos and never face such problem.
Hi,
Could you please let me know which mqx version are you using??
Regards
Sol
MQX_4_0 and using c90fl flash driver.and code got stuck when i call flash erase driver on some board and working on others.voltages are ok as i can programme same board with debugger and boot loader developed with out mqx