AnsweredAssumed Answered

CAN Receive Buffers on MKE06Z128VLH4

Question asked by Sam Kreuze on Nov 18, 2015
Latest reply on Nov 19, 2015 by Sam Kreuze

Hello,

 

I'm developing an application on the MKE06Z128VLH4 which will use CAN for communication. In KDS I added the CAN_LDD component, configured it, and generated code. I am able to communicate via CAN using this module.  Now I would like to add another CAN RX Buffer to the component. In the Component Selector for CAN_LDD ->Settings->Message Buffers, I add a receive buffer but it will not allow it because it claims "CAN device supports only 1 receive buffer/s."  However, in the reference manual for this processor it claims "Five receive buffers with FIFO storage scheme"

 

I can add 3 transmit buffers to the component like the reference manual says.

 

Am I using the wrong component? or is this an issue with processor expert? or is there something I'm missing?

 

Thanks in advance,

Sam

Outcomes