MCIMX6U7CVM08 BSDL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6U7CVM08 BSDL

Jump to solution
2,450 Views
hanshogendoorn
Contributor I

According the BSDL file MCIMX6U7CVM08 is the boundary scan register length 648 bits, is this correct??

I am having a lot of problems when I am using this device in an interconnect test (Jtag Technologies soft/hardware).

Device id test is passing.

 

Kind regards, Hans

Original Attachment has been moved to: MX6S_TO1.1.bsdl.zip

0 Kudos
1 Solution
2,005 Views
Yuri
NXP Employee
NXP Employee

Hello,

Below are some general considerations.

1.

  Please check  if PCIe voltages are applied :

according to footnote of Table 2-21 (Recommended connections for unused

analog interfaces) of the Hardware Development Guide, linked below ,

SATA and PCIe supplies must remain powered if boundary scan test needs to be done.

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >

2.

JTAG_MOD (SJC_MOD) should be pulled up (to NVCC_JTAG) for Boundary Scan Mode.

3.

Please check in BSDL file is correct for the i.MX6 part.

Please use the recent BSDL file from the Freescale Web :

“MX6DL_TO1.1.bsdl” file for i.MX6 DL.

https://cache.freescale.com/secured/NMG/MAD/IMX6_DL_S_BSDL.zip?__gda__=1447919960_27cec57af1ceb1395d...

Note :

“attribute BOUNDARY_LENGTH of MX6DL: entity is 648;”

4.

Please pay attention on COMPLIANCE_PATTERNS of the BSDL file.

attribute COMPLIANCE_PATTERNS of MX6S: entity is

  "(TEST_MODE, JTAG_MOD, POR_B) (011)";

Check if :

TEST_MODE is LOW ;

JTAG_MOD is HIGH ;

POR_B is HIGH.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
2,006 Views
Yuri
NXP Employee
NXP Employee

Hello,

Below are some general considerations.

1.

  Please check  if PCIe voltages are applied :

according to footnote of Table 2-21 (Recommended connections for unused

analog interfaces) of the Hardware Development Guide, linked below ,

SATA and PCIe supplies must remain powered if boundary scan test needs to be done.

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >

2.

JTAG_MOD (SJC_MOD) should be pulled up (to NVCC_JTAG) for Boundary Scan Mode.

3.

Please check in BSDL file is correct for the i.MX6 part.

Please use the recent BSDL file from the Freescale Web :

“MX6DL_TO1.1.bsdl” file for i.MX6 DL.

https://cache.freescale.com/secured/NMG/MAD/IMX6_DL_S_BSDL.zip?__gda__=1447919960_27cec57af1ceb1395d...

Note :

“attribute BOUNDARY_LENGTH of MX6DL: entity is 648;”

4.

Please pay attention on COMPLIANCE_PATTERNS of the BSDL file.

attribute COMPLIANCE_PATTERNS of MX6S: entity is

  "(TEST_MODE, JTAG_MOD, POR_B) (011)";

Check if :

TEST_MODE is LOW ;

JTAG_MOD is HIGH ;

POR_B is HIGH.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
2,005 Views
hanshogendoorn
Contributor I

Thanks Yuri,

I find out yesterday that the PCIE voltage is connected to GND , so I think I can stop debugging!

Only the device_id is read out correct.

Thanks, Hans

Met vriendelijke groet,

Kind regards/mit freundlichen Grüßen,

tbp electronics bv

Hans Hogendoorn

test design engineer

E hhogendoorn@tbp.nl<mailto:hhogendoorn@tbp.nl>

T +31187602744

@tbp: Monday to Friday

Van: Yuri

Verzonden: donderdag 19 november 2015 7:11

Aan: Hans Hogendoorn

Onderwerp: Re: - MCIMX6U7CVM08 BSDL

<http://jiveon.jivesoftware.com/mpss/c/8gA/PDcDAA/t.1s9/Wajh6HUHRUScEqDJ-BXGwQ/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

MCIMX6U7CVM08 BSDL

reply from Yuri Muhin<http://jiveon.jivesoftware.com/mpss/c/8gA/PDcDAA/t.1s9/Wajh6HUHRUScEqDJ-BXGwQ/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQuFPEPvxbIEdmXkTIJKJlvLtE60ovg1JsmwU97EV8kDnyQobvus7WCo5HCX-2B1MKb0-3D> in i.MX Community - View the full discussion<http://jiveon.jivesoftware.com/mpss/c/8gA/PDcDAA/t.1s9/Wajh6HUHRUScEqDJ-BXGwQ/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSOyR7kSuD7b-2FWroe3nZSfEUvWD4L-2BqOiWoHFWedvjONlgHUQ5dEt-2FrUd6I-2BiMxrEA-3D>

0 Kudos