i.MX 6UltraLite Ball Map

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6UltraLite Ball Map

591 Views
ricardoferreira
Contributor II

Hi,

In the datasheet of the i.MX 6UltraLite, for the 9x9 mm, 0.5 mm Pitch package the pin NVCC_DRAM_2P5 is in the position K6 and in the Table 93 is in the N6 position.

Could you clarify the position of the pin?
Thank you very much in advance.

Regards,
Ricardo F.

Labels (1)
0 Kudos
1 Reply

475 Views
Yuri
NXP Employee
NXP Employee

Hello,

The correct ball number for NVCC_DRAM_2P5 is K6.

(Documentation correction request has been submitted)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos