iMX6UL uSDHC 1 or 2 interfaces

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL uSDHC 1 or 2 interfaces

855 Views
johandeben
Contributor I

I'm wondering if the iMX6UL-1 has 1 or 2 uSDHC interfaces.

In the datasheet, I can find 2 interfaces.

But when using the Processor Expert for iMX6UL, I can only see 1 uSDHC interface.

So what is correct?

Labels (1)
0 Kudos
2 Replies

597 Views
Yuri
NXP Employee
NXP Employee

Hello,

    The Datasheet is correct - 2 uSDHC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

597 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

  See schematic page 7 SPF-28617_C1.pdf, please !
There are 2 uSDHC IPs in i.MX6ul, But SD2 signals are multiplexed with NAND Pads. So you had better refter to Reference Manual of i.MX6UL when you want to get PADs IOMUX mode.

Regards,

Weidong

0 Kudos