I use SN8000 WIFI module,which BSP should I use?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I use SN8000 WIFI module,which BSP should I use?

455 Views
yuanlong
Contributor II

Dear all,

I use SN8000 WIFI module in MCIMX6Q-SDB, which BSP should I use with android 5.02?

Labels (2)
0 Kudos
1 Reply

352 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuan

as mentioned below it is supported with Linux 3.14.38

http:/ /wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos