Hi
We have connected RGMII back to back between IMX and ZYNQ
Also we have taken care of PHY simulation in our driver.
The problem we are facing currently is while pinging "IMX <-> ZYNQ" with payload
we are seeing the packet loss.
This issue (PacketLoss) was not observed in freescale provided 3.0.35 kernel ,but is currenly observed
in 3.10.53 kernel
I have seen additional things like flow control has been added in 3.10.53 kernel
also there are few changes w.r.t tx/rx flow .
Could that be resulting in packetloss issue
Hello Himanshu,
Yes, this changes could be the result of packetloss, since as you may already known the i.MX6 FEC Controller, has an errata. Please see more details in the following link:
Hi James
I am unable to access above link
Regards
Himanshu