About the power consumption at each ARM frequency for i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the power consumption at each ARM frequency for i.MX6UL

630 Views
yuuki
Senior Contributor II

Dear all,

In AN5170, The voltage levels of VDDARM and VDDSOC is shown in following Table1.

VDDARMSOC voltage level.png

In each ARM frequency and VDDARM/VDDSOC setting,
Did each power consumption be tested?

Would you tell me the result if power consumption is tested under conditions of them?

Best Regards,
Yuuki

Labels (1)
0 Kudos
2 Replies

462 Views
BiyongSUN
NXP Employee
NXP Employee

It is a case by case measurement, which is related to DVFS. 

In the document, the test conditions are provided in each case. And the cases cover the voltage in Table 1.

The table mentioned by you are the LDO enable, which are using the internal PMU.

Untitled.png

0 Kudos

462 Views
yuuki
Senior Contributor II

Dear Biyong Sun-san,

Thank you for your support.

We changed a frequency and measured a power consumption.
(528MHz/396MHz/198MHz)
However, we were not able to see a change of the power consumption.

Is this right behavior?

Best Regards,
Yuuki

0 Kudos