Sensor Fusion Toolbox Stand alone flash on FRDM-KL25Z failing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensor Fusion Toolbox Stand alone flash on FRDM-KL25Z failing

Jump to solution
695 Views
antoinevanderhe
Contributor I

Hello All,

 

I am trying out the Freescale Sensor Fusion Toolbox (build on 11 september 2015).

 

I only got the following problem when flashing the file: FRDM-KL25Z-V-NED.hex (stand alone) to the MBED drive.

 

I am getting the error BAD EXTENSION FILE (in the fail.txt file)

 

This is on MBED with MBED firmware rev 203. Bootloader version from Pemicro is v111.

 

On which version has it been working/tested? Is there an updated file (hex/bin) available? Or any suggestion what to try more?

 

Thanks in advance!

 

Best regards,

Antoine van der Heijde

Labels (1)
0 Kudos
1 Solution
487 Views
michaelestanley
NXP Employee
NXP Employee

Antoine,

The GUI is assuming that KL25Z boards are programmed with OpenSDA V1 by P&E Micro.  That's why they won't work with your MBED-enabled board.

If you reprogram the board to the P&E interface, it should work just fine.

Regards,

Mike

View solution in original post

0 Kudos
2 Replies
488 Views
michaelestanley
NXP Employee
NXP Employee

Antoine,

The GUI is assuming that KL25Z boards are programmed with OpenSDA V1 by P&E Micro.  That's why they won't work with your MBED-enabled board.

If you reprogram the board to the P&E interface, it should work just fine.

Regards,

Mike

0 Kudos
487 Views
antoinevanderhe
Contributor I

Hi Mike,

Thanks for the quick response!

I did not realized there was a difference between the MSD loaders. It is working very fine now! Thank you.

Best regards,

Antoine

0 Kudos