AnsweredAssumed Answered

Remove login prompt in Yocto kernel build

Question asked by aznjaput on Nov 6, 2015
Latest reply on Nov 15, 2015 by aznjaput

Hello,

 

I'm trying to figure out how to disable the following login prompt after the kernel boots:

    Poky (Yocto Project Reference Distro) 1.8.1 nitrogen6x /dev/ttymxc3

    nitrogen6x login:

 

In the LTIB environment (L3.0.35_4.1.0), there was an option in the LTIB configuration to disable the login prompt:

    LTIB configuration -> Options -> [ ] boot up with a tty and login

   

I'm looking to do the same in the Yocto environment. The point of this is for an application to autolaunch after the kernel boots. I did that in the LTIB environment by disabling the login prompt and launching the application through rc.local. I'm using kernel 3.14.28 with an imx6q processor.

 

Thanks,

Outcomes