i.MX6Q U-boot splash and Linux 3.1x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q U-boot splash and Linux 3.1x

457 Views
markfeatherston
Contributor II

Can the u-boot splash persist into Linux until something actually attempts to use the framebuffer in Linux?  I've seen a few patches around for older kernels, but is there anything already implemented for later kernels like 3.10.53 or the 3.14 series?

Labels (3)
0 Kudos
1 Reply

323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

such splashscreen is reviewed on below link and unfortunately seems there were no plans for updating it

Patch to support uboot logo keep from uboot to kernel to Android for JB4.2.2_1.1.0-GA and L3.0.35_4....

Best regards

igor

0 Kudos