AnsweredAssumed Answered

L9 pin of i.MX6SoloX(17x17 mm NP)

Question asked by Zongbiao Liao on Nov 5, 2015
Latest reply on Nov 6, 2015 by Yongxin Huang

Hello Community

 

About L9 pin of i.MX6SoloX(17x17 mm NP),the information in Table 122 and Table 124 of datasheet IMX6SXAEC

is different.I want to know which is right.

 

1)In Table 122. 17x17 mm NP (no PCIe) supplies contact assignments (continued)

L9-1.PNG

 

2)In Table 124. 17x17 mm (No PCIe), 0.8 mm Pitch, 20x20 Ball Map (continued)

L9-2.PNG

 

3)Besides,in Table131(i.MX 6SoloX Data Sheet Document RevisionHistory,there is note as below:

• In Table 122, "17x17 mm NP (no PCIe) supplies contactassignments," on page 168, added ball L9 to the VDD_SOC_CAP row

 

Please tell me which is right.

 

Best Regards,

ZongbiaoLiao

Outcomes