TEST_MODE pin connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEST_MODE pin connection

Jump to solution
998 Views
ko-hey
Senior Contributor II

Hi all

I want to confirm a recommendation about TEST_MODE pin.

According to the check List and HW Design Guide, there is a following recommendation about TEST_MODE pin.

So user must float it or connect GND directly.

The TEST_MODE input is internally connected to an on-chip pulldown device. The user must either float this signal or tie it to GND.

On the other hand, SABRE isn't following the recommendation.

It connect GND through 4.7 Kohm in SPF-27616_C5.pdf.

What is freescale's recommendation ?

Please also tell me why does SABRE board not follow the recommendation.

Ko-hey

Labels (1)
0 Kudos
1 Solution
878 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

on reference board signal is routed externally for possibility to connect it to high level

(used for manufacturing tests), 4.7 Kohm is used for secure connection

to ground in emi presence. Since customer boards do not use manufacturing

tests, recommendation is to follow HW Design Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
879 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

on reference board signal is routed externally for possibility to connect it to high level

(used for manufacturing tests), 4.7 Kohm is used for secure connection

to ground in emi presence. Since customer boards do not use manufacturing

tests, recommendation is to follow HW Design Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

878 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your support.

Why does the "Float" recommend ?

I think "float" is more susceptible to external influences than 4.7 Kohm pull-down.

So the best way is connect to GND.

Is it correct ?

Ko-hey

0 Kudos
878 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes correct

Best regards

igor

0 Kudos
878 Views
ko-hey
Senior Contributor II

Hi Igor

Thanks.

Ko-hey

0 Kudos