ltib L2.6.35_1.1.0_130130; kernel panic issue while trying to load from ram.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib L2.6.35_1.1.0_130130; kernel panic issue while trying to load from ram.

607 Views
ijazfazily
Contributor III

Hi,

We are getting the following issue while trying load the image from ram. I have checked the disk image and have found the file "init" in "/sbin". I have checked that the permissions are set to allow execution. I have also checked that busybox is present in /bin and that the permissions are set to allow execution.

==============================================================================================

setenv bootcmd 'bootm 0x42000000 0x42300000' ; setenv bootargs noinitrd console=ttyAM0,115200 root=/dev/ram init=/sbin/init rootfstype=ramdisk rw ramdisk_size=10000; boot

mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:05:31 UTC (331)

VFS: Mounted root (ramdisk filesystem) on device 0:14.

Freeing init memory: 152K

Failed to execute /sbin/init.  Attempting defaults...
Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance
.

Backtrace:

[<c003212c>] (dump_backtrace+0x0/0x110) from [<c0367a94>] (dump_stack+0x18/0x1c)

r6:c004c9cc r5:c0026074 r4:c04b1500 r3:00000000

[<c0367a7c>] (dump_stack+0x0/0x1c) from [<c0367c7c>] (panic+0x74/0xf0)

[<c0367c08>] (panic+0x0/0xf0) from [<c0367a54>] (init_post+0xb4/0xdc)

r3:c7c24000 r2:c7da6b00 r1:c7da6c00 r0:c040f21e

[<c03679a0>] (init_post+0x0/0xdc) from [<c0008b00>] (kernel_init+0x12c/0x168)

r4:c0026074 r3:c7801080

[<c00089d4>] (kernel_init+0x0/0x168) from [<c004c9cc>] (do_exit+0x0/0x6b8)

r5:c00089d4 r4:00000000

========================================================================================================

But we were able to load the rootfs from nand with the following bootargs: setenv bootcmd 'bootm 0x42000000' ; setenv bootargs noinitrd console=ttyAM0,115200 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs ro gpmi; boot

Any suggestions would be really appreciated.

Thanks & Regards,

Ijaz Fazily

Labels (2)
1 Reply

405 Views
igorpadykov
NXP Employee
NXP Employee

Hi ljaz

please check below link

i.MX28: Enable initramfs step by step

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------