Information of BD-SL-I.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Information of BD-SL-I.mx6

397 Views
munishsharma
Contributor I

Hi

   I want to record 2 analog  camera's using BD - SL- i.mx6  development board.

     my Question is

     1). can i interface two camera simultaneously on considered board one is connected on MIPI port and other is connected on parallel port and possible to do parallel operation.  

     2). is it possible to stream both camera input on the screen (Hirose DF 14 -20p-1.25H) and store uncompressed both camera input on the sata device.

Thanks in Advance

Regards

Munish

Labels (1)
0 Kudos
1 Reply

330 Views
igorpadykov
NXP Employee
NXP Employee

Hi Munish

in theory both cameras can work concurrently as shows below part

of i.MX6DQ RM

1.jpg

however seems some restrictions exist for that board according to

https://boundarydevices.com/mipi-camera-support-on-i-mx6/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos