AnsweredAssumed Answered

MK60FX512 low power mode

Question asked by Francesc Xavier Pastor on Nov 2, 2015
Latest reply on Nov 16, 2015 by Francesc Xavier Pastor

Hi everybody,

 

In my application using MK60FX512 through MQX 4.1.1 I set up the clocks so that OSC0 is DISABLED, OSC1 is an external crystal of 48MHz and RTC oscillator with the typical value of 32.768kHz.

 

Then, I modify the BSP using the Processor Expert in order to configure the board with my specific clock configuration as mentioned. When I rebuild the libraries and  run the low power example, it seems like when the function "_lpm_set_clock_configuration(BSP_CLOCK_CONFIGURATION_2MHZ)" is called, the system is stuck and the application doesn't work till I reset the board stucking again and again.

 

Does anybody know if it's possible to work in low power modes using this clock configuration? In case affirmative, what am I missing in the BSP's processor expert to make it work?

 

Thank you very much in adavanced

Outcomes