AnsweredAssumed Answered

MQX MK60 virtual NIC example

Question asked by Jason Blackston on Nov 2, 2015
Latest reply on Nov 9, 2015 by Jason Blackston

With the virtual NIC example for the MK6x how do you then connect to it. You have an IP Address, but what is the Port you are suppose to connect on?

 

Also how do you enable HS-USB, if you have the board setup to support HS-USB. I don't see anywhere in the code to enable it, even in the virtual COM (CDC) code either. I'm assuming you have to make some kind o modification to add support for it.

Outcomes