Dear all,
I have a question about STOP MODE of PMU of MX6UL.
I refer to STOP_MODE_CONFIG Field of Miscellaneous Register 0 (PMU_MISC0) in MX6UL Refrence Manual.
The 0x11 setting shows "STOP (very lower power)-Analog regulators are OFF".
However, in Table 10-3. STOP mode configuration, I think that explanation of STOP_MODE_CONFIG is reverse.
I understand that explanation of STOP_MODE_CONFIG Field is right.
Is my understanding right?
Best Regards,
Yuuki
Solved! Go to Solution.
Hello,
The Table 10-3 (STOP mode configuration) is not fully correct regarding
column names :
instead of “STOP_MODE_CONFIG=0” – should be “Analog regulators are OFF”
instead of “STOP_MODE_CONFIG=1” – should be “Analog regulators are ON”.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
The Table 10-3 (STOP mode configuration) is not fully correct regarding
column names :
instead of “STOP_MODE_CONFIG=0” – should be “Analog regulators are OFF”
instead of “STOP_MODE_CONFIG=1” – should be “Analog regulators are ON”.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------