AnsweredAssumed Answered

Is there any way to boot LS2085AQDS board from UART console instead for SD card or tftp option?

Question asked by Pratik Bhatt on Nov 2, 2015
Latest reply on Nov 4, 2015 by Pratik Bhatt

Hi,

 

There is a pin multiplexing for SD card pin and I2C 2 pins in LS2085A processor, I wanted to use that pins as I2C function so SD card interface will not work.

So i want to know that is there any method to boot from out console, So i can transfer images to RAM location using UART and then boot from that RAM locations.

Is there any utility for this so i can download and use that ?

Outcomes