Vybrid Vf5xxr UART Register description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid Vf5xxr UART Register description

Jump to solution
1,288 Views
mathiaswaldenbu
Contributor I

Hi,

according to the reference manual, the UART0/UART1 include features like Initial Charachter Detection, Transmit Threshold detection and so on. But in chapter 49 (UART) of the RM, these features are not described and only registers used by all UARTs are listed. Is there a detailed manual about these features or simply a short description about the missing registers?

Thanks in advance

Labels (3)
Tags (3)
0 Kudos
1 Solution
994 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
3 Replies
995 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
995 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As I see, those features are related to the ISO 7816 smartcard support and more information regarding this feature can be found at chapter 49.4.7 ISO-7816/smartcard support.  Have you checked that part?

/Alejandro

0 Kudos
995 Views
karina_valencia
NXP Apps Support
NXP Apps Support

mathiaswaldenburger​ did you get previous comment?

0 Kudos