iMX6Q LPDDR2 MT42L128M64D2LL-25 IT_1 configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q LPDDR2 MT42L128M64D2LL-25 IT_1 configuration problem

790 Views
selvakumarvelan
Contributor I

Hi,

 

In our custom  iMX6q board we are using LPDDR2 MT42L128M64D2LL-25 RAM. The MMDC channels are configured by using the Mx6DQSDL LPDDR2 Script Aid V0.04-new.xlsx script. Please refer the attached script.

The DDR configuration is done thru DCD settings in our custom boot loader.

 

Now i load the DDR calibration tool (i.MX6/7 DDR Stress Test Tool V2.20) from my boot loader. The DDR calibartion binary image is started.

But while starting DDR calibaration it stops at Test Channel 0.

Also i attached the DDR stree test binary image log.

 

Let me know if i miss anything.

 

Thanks in advance.

 

Regards,

Selvakumar V

Original Attachment has been moved to: DDR_StressTest.log.zip

Labels (1)
0 Kudos
1 Reply

408 Views
Yuri
NXP Employee
NXP Employee

Hello,

  have You tried (to use) and change the init script (RealView.inc)

as recommended in the following thread https://community.freescale.com/docs/DOC-105652#comment-31888

Also, please look at the following : DDR stress tester V2.00 problem with i.MX6 solo lite interfacing with DDR3


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos