i.MX6Q and I.MX6DL./unused RTC_XTALI, RTC_XTALO(use spi NOR boot.)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q and I.MX6DL./unused RTC_XTALI, RTC_XTALO(use spi NOR boot.)

Jump to solution
809 Views
soichiyamamoto
Contributor V

HI,

I use i.MX6Q and I.MX6DL.

and ,I use spi NOR boot.

(I Know In addition, I know ERR007926.)

but I do not use  RTC_XTALI, RTC_XTALO.

Please tell me the unused handling of RTC_XTALI, RTC_XTALO.

Best regards,

soichi

Labels (2)
1 Solution
581 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

if 32.768 kHz external crystal oscillator is not used

RTC_XTALI can be tied to ground, RTC_XTALO left unconnected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
582 Views
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

if 32.768 kHz external crystal oscillator is not used

RTC_XTALI can be tied to ground, RTC_XTALO left unconnected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------