Hi
We use Freescale Linux LS1021A SDK v0.4 for building kernel images.
We got some errors during image building. Are these errors important?
Please see below:
After the staring the command
bitbake fsl-image-full
we received the following message:
Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-fsl-linux-gnueabi"
MACHINE = "ls1021atwr"
DISTRO = "fsl-networking"
DISTRO_VERSION = "QorIQ-SDK-V1.8"
TUNE_FEATURES = "armv7a vfp neon callconvention-hard cortexa7"
TARGET_FPU = "vfp-neon"
meta
meta-yocto
meta-yocto-bsp = "<unknown>:<unknown>"
meta-fsl-arm = "(detachedfrom5d9a9e0):error:"
meta-fsl-networking = "(detachedfrom8df6764):error:"
meta-fsl-toolchain = "(detachedfroma253b35):error:"
Regards
Victor
Use the following command sequence:
if it is 64-bit operating system, run the following command also:
sudo apt-get install ia32-libs lib32ncurses5
then choose "No" and you're done. )
bitbake fsl-image-minimal
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------