Question, i.MX28 PSWITCH handling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX28 PSWITCH handling

825 Views
Aemj
Contributor IV

Hi all,

I would like to ask about PSWITCH handling of i.MX28.

My customer is facing the issue that i.MX280 cannot startup on their two proto boards out of 30 boards.

They are using i.MX280 with 5V power supply pin opened, and feeding 3.3V to Battery pin.

To enable internal DC/DC, PSWITCH is connected to VDDXTAL directly to set PSWITCH to mid-level.

In i.MX28 datasheet, it is described as below.

“A MID LEVEL PSWITCH state can be generated by connecting the VDDXTAL output of the SoC to PSWITCH through a switch.”

(1)

Is it possible to connect PSWITCH to VDDXTAL always?

For test, they cut the connection between PSWITCH and VDDXTAL and changed the connection of PSWITCH as below.

pastedImage_0.png

Then they saw i.MX28 could boot-up normally.

But when they removed the capacitor from above circuit, i.MX28 could not boot-up(DC/DC did not start).

It seems that the rise of PSWITCH voltage needs delay.

(2)

Are there any requirements on the power-up sequence of PSWITCH?

Thanks,

Miyamoto

0 Kudos
3 Replies

460 Views
Yuri
NXP Employee
NXP Employee

Hello,

According to the i.MX28 Design Checklist, linked below,

it is not recommended to connected PWITCH to VDDXTAL directly,

as it cannot be asserted when asserting RESETN.

https://community.freescale.com/docs/DOC-98792


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

460 Views
Aemj
Contributor IV

Hi Yuri,

Thanks for your reply and sorry for my late response.

Is it possible to feed about 1V to SPWITCH during asserting RESETN?

Thanks,

Miyamoto

0 Kudos

460 Views
Yuri
NXP Employee
NXP Employee

Yes.

~Yuri.

0 Kudos