Hi,
I'm trying to run Qt5 QML apps on a imx6ulevk board.
As there is no eglfs support on the hardware side I'm trying to use the linuxfb QPA-Plugin to render via software.
But upon starting any QML app, I don't get any output on the screen.
Can someone help, please?
Best Regards,
Frieder
I just tried to run some Qt-widgets apps and they are running fine, whereas also non-qt apps with GUI, like ts_test are not putting anything on the screen.
Hi Frieder,
I have exactly the same problem as you ... I would like to execute Qt5 QML apps in the imx6ulevk and I have not succeeded so far.
Regarding QML, I got the following answer in the meta-freescale lists from Otavio Salvador:
"You can use QT5 with the i.MX6UL but without QML. The QML requires the Qt Quick 2D
raster library to work without 3D GPU and this is a commercial module from The Qt Company."
I would also like to test the graphical capabilities with opengl and openvg software renderization and cannot execute any example available in the fsl-image-qt5.
Have you done some tests to check it? Could you please help me with an indication on how to do it?
I created fsl-image-qt5 with X11 as backend.
Thanks and regards,
alvaro
Hi Alvaro,
Thank you for sharing the information. I didn't get any further with using software rendering.
I'm not using X11 or any windowing system.
I tried to use mesa as opengl software implementation, but didn't succeed so far.
I'm wondering if there is any alternative to the commercial Qt Quick 2D renderer?
Regards
Frieder