AnsweredAssumed Answered

About u-boot for UHS-I mode in i.MX6DQ.

Question asked by Keita Nagashima on Oct 25, 2015

Dear All,

 

Do you have a u-boot which supported UHS-I mode in i.MX6DQ?

 

We confirmed the Linux kernel was supported UHS-I mode in android L5.0.0_1.0.0.

(UHS-I [SDR104]: 1.8V signaling, Frequency up to 208 MHz, up to 104MB/sec)

But, u-boot wasn't supported it.

(i.e. High Speed mode: 3.3V signaling, Frequency up to 50 MHz, up to 25 MB/sec)

 

Best Regards,

Keita

Outcomes