AnsweredAssumed Answered

Camera capture at same time through IC and directly to memory

Question asked by Erez Steinberg on Oct 26, 2015
Latest reply on Oct 28, 2015 by Yuri Muhin

Dear experts,

 

I am wondering if the following is possible.

 

iMX6 is connected to a single CMOS sensor, e.g. 1080p.

 

Is it possible to have both paths working at the same time:

CSI -> MEM

CSI -> IC -> MEM

 

So, for every frame, I can get the original image from the sensor (CSI->MEM)  + a downscaled image (CSI->IC->MEM) ?

 

Can iMX6 support such a configuration in theory?

 

 

Sincerely,

Erez

Outcomes