For the 32.768KHz RTC crystal I cannot get the typ. 50K series and the 10pF load as called out in the data sheet,
So would it be better to lower the capacitance and increase the series resistance or increase the capacitance and
maintain the 50K series resistance.
Hi Reed
increased capacitance may lead to increased power dissipation in the crystal, as
noted for example in CHRONTEL AN-06:
it is not recommended that extra capacitance be added to pins XTAL1 and XTAL2
of the clock chip unless it is absolutely necessary
https://community.freescale.com/thread/337117
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------