AnsweredAssumed Answered

IPU_DI1_PIN01-17 vs IPU_DISP1_DATA00-23 how used?

Question asked by Adrian Thewlis on Oct 22, 2015
Latest reply on Oct 26, 2015 by igorpadykov

I have a board with an RGB LCD connected to the pins corresponding to IPU1_DISP1_DATA00-23 and was using the SDK sample to code to get the display working. As I was going through I noticed these two different sets of pins.

 

What is the difference between the DISPn_DATAxx pins and the DIn_PINxx pins? Are they both utilized by the DI module in IPU, and how the two mechanisms chosen between?

 

 

Other than mentioning them as external pins to the IPU, I couldn't find any other reference to the DISPn_DATAxx pins.

 

Adrian

Outcomes