Hi community,
I want to know how to calculate DISP_CLK_PERIOD and DI_CLK_PERIOD in datasheet (IMX6DQCEC Rev.4) chapter 4.11.10.6.3.
Datasheet says "The DISP_CLK_PERIOD, DI_CLK_PERIOD parameters are register-controlled.", so we can find dix_disp_clk_period in chapter 37.5.194 and chapter 37.5.230 in IMX6DQRM Rev.3.
Are these fields correspond with DISP_CLK_PERIOD?
And which register is correspond with DI_CLK_PERIOD?
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hello,
The sections 37.5.194 37.5.230 in IMX6DQRM about IPUx_DIy_BS_CLKGEN0
relate to DI_CLK_PERIOD, whereas DISP_CLK_DOWN and DISP_CLK_UP parameters
(which are set via the Base Sync Clock Gen 1 Register) define DISP_CLK_PERIOD.
DISP_CLK_PERIOD may be considered as sum of DISP_CLK_DOWN and DISP_CLK_UP
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
The sections 37.5.194 37.5.230 in IMX6DQRM about IPUx_DIy_BS_CLKGEN0
relate to DI_CLK_PERIOD, whereas DISP_CLK_DOWN and DISP_CLK_UP parameters
(which are set via the Base Sync Clock Gen 1 Register) define DISP_CLK_PERIOD.
DISP_CLK_PERIOD may be considered as sum of DISP_CLK_DOWN and DISP_CLK_UP
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------