iMX28 Battery Charger not charging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 Battery Charger not charging

Jump to solution
905 Views
MartinHo
Contributor IV

I'm having problems to enable the Battery charger on my custom Board (Running Windows CE 6.0)

The problem is that the charge current is only about 45mA@3.77V (I'm setting the Charger to 500mA, having a stable +5V Supply  with up to 1.25A)

The HW_POWER registers are:

BatteryVoltage = 3776

DieTemperature = 41

Charge Current: 0x28

HW_POWER_CTRL = 0x7054C

HW_POWER_5VCTRL = 0x2403F117

HW_POWER_MINPWR = 0x40

HW_POWER_CHARGE = 0x128

HW_POWER_VDDDCTRL = 0x2071D

HW_POWER_VDDACTRL = 0x270C

HW_POWER_VDDIOCTRL = 0x270A

HW_POWER_VDDMEMCTRL = 0x230

HW_POWER_DCDC4P2 = 0x80C20018

HW_POWER_MISC = 0x0

HW_POWER_DCLIMITS = 0x305F

HW_POWER_LOOPCTRL = 0x167021

HW_POWER_STS = 0x21178A2E

HW_POWER_SPEED = 0x800

HW_POWER_BATTMONITOR = 0x1D60E00

HW_POWER_RESET = 0x0

HW_POWER_SPECIAL_RD = 0x0

I somebody is so kind to take a look at my register settings and pointing me to the error, i would be very glad.

Regards

Martin

Labels (2)
0 Kudos
1 Solution
646 Views
MartinHo
Contributor IV

Thanks Igor

After some more test's i change the HW and magically the charger started working, I have probably broken the charger circuit on my 1. Board.

Thank's for Your help

Martim

View solution in original post

0 Kudos
2 Replies
646 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

reason may be that 4P2 LinReg and battery charger both share the 5 V current, while

4P2 LinReg is having priority, details for setting charger current is described in

attached app note sect.5 Battery Charging Subsystem.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
647 Views
MartinHo
Contributor IV

Thanks Igor

After some more test's i change the HW and magically the charger started working, I have probably broken the charger circuit on my 1. Board.

Thank's for Your help

Martim

0 Kudos