OpenMAX IL support for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenMAX IL support for i.MX6

1,350 Views
kirgene
Contributor II

Hello,

I have a multimedia software based on OpenMAX IL that runs on Linux.

I'd like to know if there any support for OpenMAX from i.MX drivers so that I can easily port this software to i.MX platform?

Thanks.

0 Kudos
1 Reply

621 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yevhen

i.mx extended multimedia feature package provides support

for OMXPlayer framework for android, not for linux.

Board Support Packages (27)

IMX6-L500-100-ANDROID-SOURCE-BSP (REV L5.0.0_1.0.0)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite and

i.MX6SX Android L5.0.0_1.0.0 BSP, Source Code for BSP and Codecs.

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos