Does Kinetis K60_100 support MII interface for ethernet connection?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Kinetis K60_100 support MII interface for ethernet connection?

Jump to solution
632 Views
lucacampanale
Contributor I

I would like to use a Kinetis K60_100 mcu, MK60DN512VLL10.

In the K60 datasheet I read "Ethernet controller with MII and RMII interface to external PHY". But the phisical RX/TX pin to PHY are only two RXD0, RXD1 and TXD0,TXD1. It should be 0:3.

Indeed when I implement the Ethernet component on the Processor  Expert, selecting interface MII, I had the following error: "target processor does not contain peripheral".

What I do not understand?

Bless you !

Labels (1)
0 Kudos
1 Solution
488 Views
mjbcswitzerland
Specialist V

Luca

The K60 supports MII Ethernet connection but you will need to chose a package with 144 pins for these options to be available.

The 100 and 121 pin packages lead-out only the RMII pins.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K60: http://www.utasker.com/kinetis/TWR-K60N512.html / http://www.utasker.com/kinetis/TWR-K60D100M.html / http://www.utasker.com/kinetis/TWR-K60F120M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

View solution in original post

0 Kudos
1 Reply
489 Views
mjbcswitzerland
Specialist V

Luca

The K60 supports MII Ethernet connection but you will need to chose a package with 144 pins for these options to be available.

The 100 and 121 pin packages lead-out only the RMII pins.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K60: http://www.utasker.com/kinetis/TWR-K60N512.html / http://www.utasker.com/kinetis/TWR-K60D100M.html / http://www.utasker.com/kinetis/TWR-K60F120M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

0 Kudos