AnsweredAssumed Answered

Processor Expert Component Name

Question asked by Richard Fox on Oct 16, 2015
Latest reply on Oct 21, 2015 by Richard Fox

My question deals with Processor Expert Component names.

 

I am using KSKD 1.3 and KDS 3.00.

 

When I look at the component repository, say KSDK_Repository\Beans,

I see a USB component named Init_USB_OTG_VAR0. When I look at

the component in the component library of the IDE I see Init_USB_OTG.

The suffix _VAR0 is missing. (I am comparing the IDE repository with

the Windows directory.)

 

I attempt to build a USB CDC project, using the USB stack component,

Processor Expert is looking for Init_USB_OTG_VAR0, and does not find

it. There are a number of components which also have a name mismatch.

(Missing _VAR0, _VAR1)

 

The USB stack is in the My Repository repository, while the OTG

component is in the KSDK Repository.

Outcomes