AnsweredAssumed Answered

MIPI camera problem on SabreLite using LTIB (L3.0.35_4.1.0_130816_source)

Question asked by raymond man on Oct 16, 2015
Latest reply on Oct 22, 2015 by raymond man

Hi,

 

I want to develop a a driver for a OV mipi camera. Before that, I do an experiment to check the signals of ov5640 mipi camera. <FSL gnome release packages> is selected to build the image files. Then I run

 

1) modprobe mxc_v4l2_capture

2) modprobe /lib/modules/3.0.35-2666-gbdde708/kernel/drivers/media/video/mxc/capture/ov5640_camera_mipi.ko

3) gst-launch mfw_v4lsrc device=/dev/video0 ! vpuenc ! fakesink &

 

I can see the clock and data signals of I2C but MCLK (produced by PWM3) is absent. Thus, there is no response from the sensor.

 

I also run Dizzy/Yocto image files (core-image-sato-nitrogen6x-20141107205431.rootfs.sdcard.gz downloaded from https://boundarydevices.com/dizzy-release-yocto/). Run the same commands and PWM3 does produce 22MHz clock signal.

 

Can anyone drop me some hints?

 

Thanks a lot!

 

Ray

Outcomes