Hello,
I use the P2020rdb from Freescale with VxWorks 6.9 and a compatible current BSP from WindRiver. When I want to activted the ECC support the boot loader did not boot anymore.
My question: Is the P2020rdb ready to use the ECC feature or not?
I ask because I found this comment in the VxWorks BSP:
/* possibly this is not supported check your DDR undefined for safety */
#undef INCLUDE_DDR_ECC
I have the P2020RDB-PCA Rev B.
Thanks in advance,
Andreas
Have a great day,
The P2020RDB-PCA rev.B is not ready to use the ECC feature. It has 64-bit DDR memory (4 x 16-bit DDR devices). There is not DDR memory device for ECC on the P2020rdb nor place to install it.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------