I am unable to install Codewarrior 5.1 Special (CW_HC12_v5.1_SPECIAL.exe. It will never finish. Computer Lenovo ThinkCenter M93p. 8Gb RAM. Intel core i7 -4765T @ 2.00 Ghz Windows 7 Enterprise sp1 64 bit. This occurs on all 5 like computers. Please help!
Hi Bob,
In addition to Jennie.
I think the installer should work on all 64 bit OS.
Is it linked to another tool ?
I recommend you to disable the anti-virus during the installation and to install it using administrator user right.
If this is not working may be the installer file is corrupter and you can try to re-download it.
Else you can install the tool on another PC, copy the installation folder and execute the \bin\regserver.bat file.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Bob
officially CW5.1 supports this platforms:
Host platforms
Microsoft windows Xp 32 & 64 bit (professional edition)
Microsoft windows Vista 32 & 64 bit (business)
Microsoft windows Vista 32 bit (Home premuim)
Microsoft windows 7 32 & 64 bit (professional edition)
Microsoft windows 7 32 & 64 bit (Home premium)
Enterprise edition is not supported officially.
does this answer your question?
Jennie
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------