I can use usb tap and cw 10.4 to program nand flash on my board based on 8309 sucessfully, but failed to use cw tap and 10.4, why?
Test connection using the following command sequence:
Connection Server from your Windows' Start->Programs menu. When the CCS icon appears in the Windows Tooltray, double-click it to bring up the CCS Console. At the CCS Console prompt, enter these commands and send me your results:
clear
show ver
pwd
findcc cwtaps -usb
findcc cwtaps
source IDcode.tcl
1 <------ selects your CWTAP via USB connection
show cc
scanboard
Can CodeWarrior connection server find the CodeWarrior TAP using “findcc” command?
Can codeWarrior TAP detect connection to the MPC8309 board using “scanboard” command?
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello jianmin lv,
What's the failure, can you please show the error log?
Have a great day,
Lunmin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------